nVent esittelee korkean tehon säilytysteknologian uudella nVent RAYCHEM HTV -lämpökaapelilla
LONTOO – (BUSINESS WIRE) – nVent Electric plc (NYSE:NVT) (”nVent”), sähköliitäntä- ja suojausratkaisujen maailmanlaajuinen markkinajohtaja, tuo tänään markkinoille uusimman itsesäätyvän lämpökaapelinsa, nVent RAYCHEM HTV:n. Uutta lämpökaapelia käytetään kriittisissä teollisissa sovelluksissa, joissa lämpötilat ovat korkeita. With superior levels of high power retention during a design life of more than three decades, the brand new self-regulating heating cable, nVent RAYCHEM HTV meets stringent demands for maximum process integrity while protecting people, processes and infrastructure.
“Growth in specialty polymers, new lightweight materials, biofuels, recycled goods, and innovative chemical processes demand heating cables that can operate at increased temperatures for prolonged periods,” said Brad Faulconer, President of nVent’s Thermal Management business. “The HTV cable brings together the most efficient materials and the latest research and development to deliver a heating cable that can meet these requirements.”
Increased performance, extended design life
nVent RAYCHEM HTV surpasses previous heating cables in performance and design life. The heating cable is specifically designed for high temperature environments and retains unparalleled levels of power output. This not only reduces downtime risk and maintenance costs for decades, it also increases plant safety and productivity. Moreover, thanks to HTV’s longer design life, its environmental impact is reduced.
New materials and ground-breaking research and development
To create such a high-performance heating cable, nVent turned to new materials, as well as research and development. With 50 years of expertise in material science and recent innovations in nanotechnology, nVent has developed a brand new semi-conductive polymer nanocomposite material that sets a new standard in power output retention and longevity.
nVent RAYCHEM heat tracing cables are already well-known for their superior protection against freezing, and maintaining critical process temperatures in many industrial facilities around the world. Its name is associated with reliability, superior performance and long operational life.
The new nVent RAYCHEM HTV self-regulating heating cable will add a whole new dimension to this reputation. nVent offers industrial plant owners the chance today to lift their process integrity and operational efficiency for decades to come.
The nVent RAYCHEM HTV heating cable will be available in Spring 2021.
Esittelyssä nVent
nVent on johtava maailmanlaajuinen sähköliitäntä- ja suojausratkaisujen toimittaja. Uskomme, että kekseliäät sähköiset ratkaisumme mahdollistavat turvallisemmat järjestelmät ja turvallisemman maailman. Suunnittelemme, valmistamme, markkinoimme, asennamme ja palvelemme tehokkaita tuotteita ja ratkaisuja, jotka yhdistävät ja suojaavat joitakin maailman herkimmistä laitteista, rakennuksista ja kriittisistä prosesseista. Tarjoamme kattavan valikoiman koteloita, kytkentäpakkauksia sekä kiinnitys- ja lämmönhallintaratkaisuja alan johtaville brändeille, jotka ovat saaneet tunnustusta maailmanlaajuisesti laadun, luotettavuuden ja innovoinnin johdosta. Päätoimistomme on Lontoossa, Isossa-Britanniassa ja Yhdysvaltain hallinnointitoimistomme Minneapolisissa, Minnesotan osavaltiossa. Vahva valikoimamme johtavia sähkötuotemerkkejä juontaa juurensa yli 100 vuoden ajalta ja sisältää tuotemerkit nVent CADDY, ERICO, HOFFMAN, RAYCHEM, SCHROFF ja TRACER.
nVent, CADDY, ERICO, HOFFMAN, RAYCHEM, SCHROFF, TRACER ja NUHEAT ovat nVent Services GmbH:n tai sen tytäryhtiöiden omistamia tai lisensoimia tavaramerkkejä.
View source version on businesswire.com: https://www.businesswire.com/news/home/20210208005135/en/
Koen Verleyen
EMEAI Marketing Manager
nVent
+32(0)478904219
[email protected]
Eugene Ho
NAM Marketing Manager
nVent
+1-650-474-7508
[email protected]
Kang Wang
APAC Marketing Manager
nVent
+86-21-24121567
[email protected]