Skip to main content
Please Select Your Country/Language Preferences

Search for nVent products, resources, or ask any question you have

Partner with nVent to Mitigate Bus System Emergency Outage and Reduce Loss

featured stories
Partner with nVent to Mitigate Bus System Emergency Outage and Reduce Loss

nVent recognizes your bus system emergency outage as their own.

emergency services

When your operations slow or cease for any reason other than a total power outage, it constitutes a full-fledged bus system emergency outage. Downtime is lost money. When thousands to millions of dollars are at stake, you need a response team that can react quickly to remedy the issue immediately. You simply can’t afford not to.

That’s why nVent recognizes your bus system emergency outage as their own. Our capabilities as a bus system manufacturer provide our field technicians with a vital advantage over service-only contractors. Our goal is to get your plant back on line as soon as possible.

Consequences of Bus System Emergency Outage

Transformer failure can grind operations to a halt, causing a ripple effect throughout a power plant. A downed transformer can be catastrophic with severe consequences that could lead to management dismissals, lawsuits, and angry stockholders. When power generation is no longer viable from a faulty transformer, getting the transformer back online has to be done with haste and with a reliable service partner.

The truth is that responder failures do occur, particularly for older facilities that have been in operation for years. A study from the University of Zagreb found that the average life cycle of a transformer is 40 years. Thus, any plant with transformers hovering around this age should be concerned. Years of heat and moisture infiltration that leads to insulation break down are a common cause for shortages on these older parts. Just one fault can cause an entire plant to go down and result in devastating financial losses. A proactive approach can protect you when—not if—a transformer problem occurs.

To curtail losses, it’s important to have a solutions partner ready to act in the case of emergency transformer replacement. Enclosures that protect this vital equipment typically house other gear that can hinder replacement line-up. Thus, the new transformer must be the same form, fit, and function of the existing equipment to ensure quick recovery. When attention to details can translate to a quick, cost-effective plug-and-play solution rather than a lengthy and costly replacement process, nVent is the partner to turn to.

Available Repair Technicians Are Ready to Get You Back Online Fast during a Bus System Emergency Outage

Unlike service-only contractors, nVent is a bus manufacturer that offers emergency repair services, employing seasoned, professional technicians that have the expertise to quickly bring your plant back on line. Our personnel is on-call 24/7 and typically respond within an hour. No other provider in the industry can match the full-response capabilities of nVent.

nVent provides:

  • Emergency repairs for Isolated Phase Bus, Non-Seg and Segregated Phase Bus
  • Transformer failure emergency services, including GSU, AUX, and MPT transformer changeouts
  • Troubleshooting expertise and root-cause analysis

nVent in Action 

With more than 50 years of experience, nVent is uniquely qualified to be there when a transformer emergency occurs. In fact, our breadth of experience, knowledge, and capability helped to resolve an emergency situation at a major power plant in Saudi Arabia.

When an explosion on a critical 864 MVA generator step-up transformer (GSU) damaged a transformer and gas-insulated line that connects the transformer to a 380-kV gas-insulated substation, we have dispatched the local Country Manager to the site to assess the situation. Damage photos and instruction book drawings were directed to the High Voltage Bus Systems (HVBS) division to create a solution. HVBS then dispatched a Field Services Manager to the site to take detailed equipment measurements to ensure a design that provided the best solution for quick recovery.

Due to the severity of the transformer fault and collateral damage, repairs to 36 sections were required to bring the generator back on line. This presented a huge logistics and manufacturing undertaking, as new components were needed to remedy the problem. Fortunately, we maintain an emergency supply of standard GIL components and boasts the in-house capability to produce additional components. nVent was able to provide the needed components within days. Air freighted via 747, a total of 22 tons of nVent high voltage transmission equipment was transported to Saudi Arabia in a 48-hour transit that normally takes 8 weeks from origin to destination.

Typically, an endeavor of this magnitude would take 5-6 months to accomplish. nVent, however, was able to complete repairs, installations, testing, and more, bringing the plant back to normal operations in less than 39 days, just in time to meet mid-summer peak demand.

As a leading provider of application-critical equipment, highly engineered technologies, and specialized services, nVent makes a difference for customers around the world. Simply put, nVent helps to mitigate damage subsequent to emergency situations, getting clients swiftly back on line with minimal losses. 

To learn more about our high voltage bus underground installation, as well as our other offerings, visit Bus Systems and Bus Services

CONTACT US


Request More Information 

To receive a quote or request additional information, use the button below to access the appropriate contact form. 
Request More Information

Bus Duct Condensation Control

Bus Duct Moisture Control: Maintaining Optimal Performance

A safe and reliable electrical bus system is an integral component of any successful power generation facility.

Learn More